This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25723: BQ25723 机械按键控制Vsys关断与开启

Part Number: BQ25723

您好,请让我咨询你个硬件开关使能/关闭BQ25723 VSYS电的问题:

           设计需求: Vin  15v, Iin max 10A ,       Vcharge:3 cell   Icharge  10-12A,筛选出BQ25723作为充电IC。

           但是设计系统开关按键时,遇到了问题:BQ25723不支持硬件开关使能/关闭BQ25723 VSYS电!!!

           我们希望硬件开关可以做到:按下硬件开关后,BQ25723可以进入低功耗模式,Isys被限流到uA极别;再按硬件开关到高电平,可以打开Vsys电。并且适配器和电池情况下都适用。

           目前看BQ25723手册,仅电池情况下支持低功耗模式,并且必须通过I2C软件配置寄存器配置进入performance mode。

           请问有没有功能与BQ25723类似,满足设计需求,但是同时支持硬件开关 设置 low power mode 和performance mode 进行切换的充电芯片  (按键功能类似笔记本电脑的开机按键功能)