Part Number: LM2611
自己产品需要将5.8V转为-5.4V,采用LM2611芯片设计实现,电路图见下方:

之前采用22UH-2.2UF-22UH,测试Vsw图像见下

测试上点电压波形,22UH-2.2UF-22UH电路配置上电过程存在类似10UH的电压波形Vsw(黄色)

更改为10UH-1UF-10UH(L5=L6=10UH,C28=1UF),测试Vsw图像见下

问题:二者为何存在差异?10UH这个波形方波间跳变是否可以正常应用?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
在datasheet第十二页有给出2个模式下的波形(图19、20),你可以对比下,第一是PWM模式或者是CCM模式, 而第二个是非连续或者是轻载下的SW波形,这是没有问题的。
变动电感有这种变化,意味着刚好处于模式临界,即便有这种波形变化并没有问题。