您好,我们使用LM5122开发 12V->24V产品,输出电压就是标准的24V,为了补偿大功率时的线损,我们考虑加入可调电阻器。
我们希望在+-2V之间实现小范围的可调,也就是24V基础上实现+-8.3%的调节范围,不知道这样环路是否会稳定呢?
是否可以给我们一个建议,在多大范围内可调会比较好呢?我们是4相并联的,大约输出电流60A左右。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我们使用LM5122开发 12V->24V产品,输出电压就是标准的24V,为了补偿大功率时的线损,我们考虑加入可调电阻器。
我们希望在+-2V之间实现小范围的可调,也就是24V基础上实现+-8.3%的调节范围,不知道这样环路是否会稳定呢?
是否可以给我们一个建议,在多大范围内可调会比较好呢?我们是4相并联的,大约输出电流60A左右。
HI
按照24V输出设计即可,+/-2V的调整没有问题。
固定补偿一般不建议做输出可调,但是小范围调整并没有问题。