This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40057: 输出效率只有77%

Part Number: TPS40057

RT,19.7V输入 5V输出,电流为20A,效率只有77怎么办啊?太离谱了,

Q1为2颗M3006D,Q2为1颗。

L1为SER2918 4.7UH。

救命!!!!附上layout图

MOS 参数为 30V 80A RDS 5.5mr Q 20nc