This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24074: CHG (BQ24074 pin9) 不拉low

Part Number: BQ24074
Other Parts Discussed in Thread: BQ28Z610-R1, , BQ28Z610

您好

我們用 BQ28Z610-R1, BQ24074 的這個線路在某些機器會發生設定 shipping mode 之後的第一次充電時 CHG (BQ24074 pin9) 不拉low維持hi-Z 的狀況。

請教你有什麼看法,為什麼會發生這樣的現象?

看起來像是shipping mode  Wake up from charging 後

被判定Battery absent 模式

MCU 沒有控制燈號,LED直接接 CHG.

Battery absent 是因為 MOS 來不及從 shipping mode 打開?

並不是每一塊板子都有這樣的問題。

電路圖如下

TP01S041A1電路圖 2022.09.15.pdf

  • 您好,正在查询,稍后回复。

  • 您好,请参考下面的内容

    Can you clarify how the system is being put into ship mode? Neither the BQ24074 nor the BQ28Z610 have a shipmode feature implemented within the IC.

    For the BQ24074 portion of the schematic, are the /PGOOD and /CHG pins pulled up to a voltage? I only see a resistor pulled up to some signals DC_OK and CHRG_OK. As these pins are open drain outputs, they do require a voltage pull up. 

    I'll look for feedback regarding the BQ28Z610 portion of the schematic. 

    It looks like the chip in shipping mode Wake up from charging, but determined battery absent mode.

    How is this being determined?

    On the charger size, are you able to provide a voltage waveform on the ISET pin, VBAT pin, and /CHG pin?

  • hi hello

    1. Answer] We use command “AltManufacturerAccess() 0x0010 SHUTDOWN Mode” to set BQ28Z610-R1 to shutdown mode, before shipping.

    2. Yes, /PGOOD and /CHG are pulled up to 3.3V via a resistor and an indication LED.  We observed that /CHG does not pull low (no LED light) on some of the PCBAs.  Not every PCBA has such behavior when wake up from shutdown mode. 

    Now the 1.5k ohm on the charging board circuit diagram should be 0 ohm (you can also directly remove the resistor), there is a resistor and LED on our side of the MCU board to 3.3V.

  • 您好,正在查询,稍后回复。

  • 您好,We observed that /CHG does not pull low (no LED light) on some of the PCBAs.  Not every PCBA has such behavior when wake up from shutdown mode.