Part Number: TPS6594EVM
问题1:
TPS6594有两个IIC,第二个IIC设备IIC2负责Q&A模式下与TPS6594通信,但是我们硬件上因为某些原因导致的第二个IIC设备不可用,那么,是否是可以将对应的GPIO1、GPIO2设置为普通IO口,那么,是否是可以通过第一个IIC设备的总线操作访问第二个IIC设备呢,如果可以的话,在这种情况下,与正常访问第二个IIC设备有什么差别吗,是否可以正常完成在Q&A模式下的喂狗操作。
问题2:

按照手册中的此张图描述,整个window1和window2的时间是确定的,那么各个写入answer的操作之后的红色箭头所指的时间间隔是否有要求呢,在手册中并未发现对于此间隔的描述,因此,是否可以理解为写入answer3、answer2、answer1之间并不需要时间间隔