我想自己手动搭接一个BUCK型的开关电源,不使用电源IC芯片,所有参数自己根据指标设定。但是我发现MOS管的驱动很难搞,请问哪些大神手动搭过这样的电路啊,关于驱动有什么解决方法吗?我用的模型就是基本的BUCK,dc/dc降压模型,你们有什么好的方案吗?谢谢了,小弟感激不尽!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好 可以使用nmos加pmos来解决驱动问题pmos作为开关管从而控制电路的通断(即后面电感电容等电路),nmos用来驱动pmos 的通断(即解决了低电压控制的问题),用5伏的电压就可以驱动nmos 的开通,最好在pmos的gs之间加个稳压二极管,从而使pmos稳定导通,在nmos的gs之间加个电阻,可以提高nmos 的关断速度,如果单片机的电压为3.3v可以用个74hc系列的芯片来驱动nmos ,解决这个问题也是我想了好几种方法,最终确定的方案,期间测试过,100khz的pwm频率,电压与占空比是线性相关的