HP-IDP480 PQ3220-PFC电感.pdf
在设计一款UCC28060交错式PFC,480W,在计算电感是280UH,匝比是8/1,但是装上去试,带一半负载(240w左右)可以,超过240W电感有响声,马上要出样品,比较着急!请问前辈是什么问题?附件为电感图纸
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HP-IDP480 PQ3220-PFC电感.pdf
在设计一款UCC28060交错式PFC,480W,在计算电感是280UH,匝比是8/1,但是装上去试,带一半负载(240w左右)可以,超过240W电感有响声,马上要出样品,比较着急!请问前辈是什么问题?附件为电感图纸
HI
240W的时候,有有没有确认电路的波形上是否有异常?
另外有没有更换更大功率的电感来验证(饱和电流更大)?
感谢你的解答!现在输出感量降低到135uH,可以满载工作,90V输入频率70K左右;(没改之前负载超过5A,90V时频率就会低于60K,波形有振荡带不动负载);但是现在有个新的问题,满载冲击几次就会击穿两个MOS管就会被击穿短路,不知道是不是因为感量的降低的问题导致还是别的问题,还请帮忙解答。
HI
感量略有影响不是重点,重点是电感饱和电流或者说功率足够大。
烧MOS很可能是电感饱和导致的。
你好,这几天一直在调试,发现是PCBlayout有点问题,修改PCB就没有炸管子了;但是现在测试PF值功率因数比较低(见图片),请这个芯片的PF值调试哪个地方?变压器是24/3T,LP=160uH
HI
逐个确认,layout, 输入电容,电感,以及电流侦测都应该有影响。