Other Parts Discussed in Thread: UCC28C40, UCC24610, UCC24612
UCC2897A看规格书仅能用到120V,如果不监控输入电压,可以将输入电压拓展到400VDC吗?或者有没有合适的IC推荐,用于给电压14V-30V的电池充电。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
可以用于超过110V以上的直流输入电压,只要将高输入电压做个电压转换使其低于110V给到芯片Vin即可,TI又提供很多110V以上输入的参考方案,你可以看看: www.ti.com.cn/.../PMP7413
有输出30V的单管正激同步整流芯片推荐吗?,MOS的DS两端电压最高可达200V
Hi
没有供电15V以上的。如果时电压很高,做个电压转换到5V左右供电UCC24610/2即可。