This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS57060-Q1: TPS57060QDGQRQ1的输出电压精度是多少,并提供相关技术资料

Part Number: TPS57060-Q1


hi Ti engineer,

TPS57060QDGQRQ1的输出电压精度是多少,并提供相关技术资料?

我们VECU控制器目前会报一些电压异常的信号,还请支持提供,谢谢!

  • HI

         一般这类芯片反馈基准精度1%, 反馈电阻精度1%, 所以最差的torenrance是不到3%, 实际一般都是在2%以内,符合绝大部分电源供应5%的供电要求。

        同时建议你确认一下输出电压波形,看是否是电压不稳定造成的?  一般不应该是精度温度造成的。