This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

太阳能充电器问题

Other Parts Discussed in Thread: BQ24650, BQ78412

我有两个问题请帮我解答下好吗

1   bq24650 能用太阳能板为 24V 100Ah 的铅酸蓄电池充电吗? 如果不可以,请推荐一款芯片好吗?充电电流不小于8A 。

2   请推荐一个电量监测芯片,用于 24V 100Ah 的铅酸蓄电池,充电电流不小于8A ,工作电流3A,峰值放电电流30A。

                                  期待回复,非常感谢!

                                                                                    成都英菲信 程红伟

                                                                                                  2013.07.29

 

 

  •  

    求回复,急需啊,谢谢啦!!

     

     

     

     

     

  • 关于充电器,BQ24650是符合你的要求的。

    关于电量管理计,这个提供一个系统架构的思路供你参考--建议你考虑BQ78412.它是专为12V铅酸电池包设计的,可以以12V铅酸电池作为一个pack ,2个pack堆栈设计,顶端板子的电流采集需要一个隔离耦合的方式采集下端sense电阻上的电流,由于其地址可以配置,所以可以考虑通过芯片的红外通讯的模式进行隔离的数据传输。

  • 关于充电器,BQ24650是符合你的要求的。

    BQ24650 的输入电压只有28V, 太阳能板的工作电压为30V,开路电压为35.2V,  另外,BQ24650的输出电压最高只有26V(实际最高可能只有25V), 这个电压能为24V铅酸电池充电吗?          我看到其他24V铅酸电池充电器的输出电压都为27.5V至28V。       BQ24650 能行吗?

            非常感谢你的解答!谢谢!!

  • 充电电压的部分,根据温度调整充电电压能够增加铅酸电池的使用寿命,如果不作为温度补偿,使用寿命会降低一些,但这个不是关键性的因素,如果你的太阳能板电压超出了芯片最大输入电压,那么只能采用集成度没有那么高的UC3909,再在外面搭配一款单独的MPPT算法芯片。