Other Parts Discussed in Thread: BQ24296
你好,
电池过放后,电池端电压为0,外接充电器无法充电;看log系统读出来的为4.2V(系统ADC读取Vbattery这个点的电压),系统判断为满电了,但是实际上电池电压是0V,请问一下是什么原因造成这个电池电压为0,但是系统读出来却是4.2V的现象的?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,The battery voltage reading from the ADC is the BAT pin voltage. Check your IBAT (battery current) to see if the battery is being charged properly. Additionally, take a look at this section of the datasheet pictured below for more information on over-discharged batteries:

If your battery is not receiving the correct ISHORT charge current, make sure that there is no external circuitry or built-in battery protection disconnecting the battery terminal from the VBAT pin.