This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD3138: downloaded the firmware ,but it failed to compile

Part Number: UCD3138


I bought an evaluation board of ucd3138evm-150, but I downloaded the firmware program of LLC to CCS, but it failed to compile

The error is as follows:

"C:/Users/22326/Desktop/xinjian/Firmware/Device/UCD3138/Linker/cyclone.cmd", line 70: error #10099-D:
program will not fit into available memory. placement with alignment fails
for section ".text" size 0x829c . Available memory ranges:
PFLASH size: 0x7f38 unused: 0x7a08 max hole: 0x7a04
error #10010: errors encountered during linking; "UCD3138_LLC_HB.out" not
built

>> Compilation failure
makefile:177: recipe for target 'UCD3138_LLC_HB.out' failed
gmake: *** [UCD3138_LLC_HB.out] Error 1
gmake: Target 'all' not remade because of errors.

 

Why?