This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65000-Q1: 关于为CMOS传感器供电转接板输出电压异常的问题

Part Number: TPS65000-Q1


我有一块开发板和一个SONY的摄像头,开发板的CSI接口输出5V和3.3V而摄像头需要2.9V 1.1V 1.8V供电。

为此我参照TPS65000-Q1规格书设计了一块转接板进行电压转换。

原理图如下:

但当我实际测量电压的时候,发现VLDO2的输出大概是2.2v,并且测量R6的阻值为230KΩ左右,R7的阻值为124KΩ左右(我有确认过这两个电阻的阻值是正常的)

也试过别的阻值匹配,例如R6 200KΩ  R7 100KΩ的情况 或者单个阻值增大增小的情况 VLDO2的输出始终不低于2V

其他的电压输出是正常的。