This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5430: TPS5430 低压9V可以正常启动,高压10V以上启动不起来

Part Number: TPS5430


和之前论坛有个问题现象非常相似,TPS5430 低压9V可以正常启动,高压10V以上启动不起来

10V以上启动输出0.6V左右,芯片不工作。

  • Hi

         轻载下呢? 或者更换饱和电流更大的功率电感?

         同时建议你确认一下layout,建议严格参考datasheet,注意功率回路尽量小,这个会印象带载能力。对于降压芯片而言,输入电压越高,功率电感峰值电流越大。