This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP87524P-Q1: LP87524PRNFRQ1

Part Number: LP87524P-Q1


在datesheet上的第14页,我看到输入电压范围与输出电压范围的关系(VOUT RANGE (V) ):

0.6 to 3.36 (VIN = 2.8 V - 4 V)

1.0 to 3.36 (VIN = 2.8 V - 5.5 V)

如果我想输出一个0.6V的电压,输入电压是否必须小于4V呢?如果使用5V输入电压输出就无法达到0.6V呢?