This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79631-Q1:

Part Number: BQ79631-Q1
Other Parts Discussed in Thread: BQ79616, , BQ78PL114

1.BQ79631-Q1的方案正适合我需要的钛酸锂电池(串起来总共最高150V电压)管理方案框图,是否还有其他类似的方案?BQ79631还需要其他的芯片(比如BQ79616或者BQ79656等支持),是否还有芯片更少的方案?

2.BQ79631-Q1的方案是否有库仑计功能?即电量计算。

3.BQ79631只能和提到的BQ79616或者BQ79656组成我需要的方案,还是BQ79631也可以和其他芯片组成我需要的方案?比如BQ79631+bq78pl114.

谢谢

  • 您好

    1,串电压最高150V,没有单颗芯片支持这么高。都是建议两颗芯片堆叠。

    2,BQ79631-Q1是电压,电流检测器,计算电量需要搭配MCU

    3, 不支持BQ79631+bq78pl114

  • 1.高电压是采取堆栈方式解决的,我说的150V是指:比如10个电芯为一个电池模组单元,5个模组串起来就堆栈出高电压了。我的意思是否可以用一种芯片+MCU就可以完成。比如

      BQ79631-Q1先做成电池模组单元的电池管理,再5个模组单元串起来。

    2.BQ79631-Q1的资料看不到,而重要的BQ79631EVM讲的感觉晦涩难懂,我搞了20年的硬件都感到整理起来都看不明白。比如BQ79631-Q1的第一页中的图就看到系统简化图,正是我需要的方案,但是BQ79631EVM里面好像看不到这个系统的原理图构造。而BQ79631EVM的第8页中的图3-1也正符合我的需求,但是后面看不到这个图的具体实施原理图。   所以看麻烦把BQ79631-Q1的堆栈应用资料发给我一下。谢谢

    3.提到的计算电量需要MCU ,那就是说电量需要自己在MCU里面建模型自己处理?而没有自带电量计算模型的类似BQ79631-Q1的高电压方案?

    谢谢

  • 着急等,谢谢

  • 您好,这款芯片完整的数据手册需要您自己申请,

    申请更多信息

    可提供完整数据表和其他信息。立即申请

    由于无法查到完整的数据手册,我需要询问更了解这款芯片的TI工程师,再帮您解答,稍后回复。

  • 您好,The BQ79631 is not a battery monitor but a pack monitor. It is used to monitor your pack+ and pack- connection as well as do UIR sensing. If your customer is looking to monitor 10 battery cells and stack them together I would advise them to use the BQ79616.