我设计的电源发现,提供1.26V电压的芯片在上电后出现发烫的现象,我用的是LM2576S提供3.3V电压,76801提供1.26V电压,通过一个三极管控制先提供1.26V电压给DSP内核,然后提供3.3给DSP外部端口。这样的组合可以使DSP正常稳定工作,但是常发现上电不久1.26V供电芯片76801很烫,不知道是不是有更好的电源设计呢?请高手指点一二。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我设计的电源发现,提供1.26V电压的芯片在上电后出现发烫的现象,我用的是LM2576S提供3.3V电压,76801提供1.26V电压,通过一个三极管控制先提供1.26V电压给DSP内核,然后提供3.3给DSP外部端口。这样的组合可以使DSP正常稳定工作,但是常发现上电不久1.26V供电芯片76801很烫,不知道是不是有更好的电源设计呢?请高手指点一二。
你好,
1,请问输入电压Vin是多少?
2,如果有空板子的话,请先不焊DSP,只给TPS76801加死负载看看会不会发烫(这样也可以避免由于意外损坏DSP).
Hi
按照您的选型TPS76801 1A输出的LDO, 也就是说你的DSP 电流功耗比较大,选择LDO时,注意需要选择热阻非常小的LDO.
假设负载电流时0.5A, 按照25℃的环境温度,PWP封装的TPS76801温度是25+0.5*(3.3-1.26)*32.6=58℃(很明显D封装的TPS76801 热阻172℃/W,环境温度25℃下,最大功耗只有568mW,而并不适合使用,25+0.5*(3.3-1.26)*172=200℃)
如上,如果您选择TPS76801,一定要选择PWP封装封装的,具体的功耗温度,可以依据你的实际情况进行计算。LDO温度取决于功耗(输入输出压差*输出电流)与热阻,你可以从这两方面着手改善。
我的输入电压是5V,空板子有,但是我还没有这么试过,空载的话应该试不出效果是吧,必须加个负载,我试一下看看吧
你这个LDO是什么意思哦?新手不太懂啊,恩看来我已经选错了 我用的是D封装的,有没有更好 更稳定的选择呢?