This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求推荐输出电流为2A或者以上的MOS驱动芯片

Other Parts Discussed in Thread: UC3845, UC3706, UCC27324, UCC27323, TPS2828

推挽电路采用电流模式,PWM芯片为UC3845,后级驱动本来为UC3706,但是UC3706输出电流最大为1.5A,计算出的所需驱动电流为1.8A,因此,求推荐一款UC3706的升级版驱动芯片。最好可以和UC3845搭配使用。
谢谢!