如题,如果不能,有无其他电源芯片替代,最好有EN和POWERGOOD
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
TPS54620可以实现1V/5A输出,你可以用webench仿真得到电路图,见官网: http://www.ti.com.cn/product/cn/tps54620
Hi
这个取决于输入电压,如果压差比较大,软件可选择的频率越低,例如12V左右输入最高频率就在700kHz左右,但是如果压差比较小,如只有3V左右,可选频率就可以到1.2MHz.
这个是软件的设置,可能是基于电源型号的选择,从仿真的参数看,电感都没有选择得非常小,所以在频率上有设限制。因为频率越高,电感越小,而压差越小,电感是越大的(在输出电压与负载一定时)。