Other Parts Discussed in Thread: TPS54140, TPS40200
请教高手,由7.4V锂电池供电,想输出一个-12V的电压,电流在200mA以内,外围尽量简单,麻烦推荐一款芯片,
最好是隔离的。
谢谢!
不知道TI有没有类似美信的MAX765的那种单芯片反相输出开关稳压器?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果是选型的话,你这种要求隔离且正负12伏的要求属于典型的flyback拓扑应用。
你可以到我这里给的选型手册中寻找flyback,且输入电压在例如4〜15,这样子找出来的基本可满足你的要求。
然后你再考虑你的其他次要要求,例如价格等从中筛选适合你的就可以啦。
选型可参考:http://www.ti.com/lit/sg/slvt145m/slvt145m.pdf
您好,我根据你的需求帮你选了一个方案(PMP2447):
(1)输入电压:4.5~15V;
(2)输出+12V和-12V两路,输出电流为400MA;
(3)芯片料号是TPS40200;
(4)拓扑属于带变压器隔离。
按照你上面的描述应该完全可以满足你的要求,你好好看看吧,有什么问题可以继续提问。
有电路图,不过这会好像传不上来,一会儿再试试。
备注:电路图上写的是PMP1278,在TI官网系统查询的时候查2447。