请教大虾们,TPS62730是怎么工作的,和CC2540使用时是什么控制使能脚的,具体工作原理是什么,为什么我的在连接的时候,松开按键就马上自动断开和PC端的连接呢?如果没有TPS62730的时候我的程序是12S才自动断开的,请问这是为什么?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
和CC2540配合工作时,可以使用CC2540的GPIO(Datasheet上的“21 General-Purpose I/O Pins (19× 4 mA, 2×20 mA)”)去控制TPS62730的ON/BYP引脚。具体工作原理可以参考TPS62730数据手册第5页的功能框图,当以下两种情况发生的时候:
1. ON/BYP为低;
2. VIN低于VITBYP时。
芯片工作在BYPASS模式中,表现为,VIN和VOUT之间通过一个2.1ohm的电阻短接起来。
你可以在调试程序的时候使用示波器观察ON/BYP的状态,确定其工作在你想要的状态,没有由于ON/BYP的变化,而使CC2540发生Reset。