This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

REF1004-2.5V



按手册采用5V输入,输入电阻50K,然后接REF1004,输出是2.5V,但是,我又在2.5V处,串接来个电阻对地,俩个电阻之间输出2V,但是在输出2V时,稳压端下降至2.45V,俩个电阻都是k欧姆级别电阻

  • xingwei li 说:

    按手册采用5V输入,输入电阻50K,然后接REF1004,输出是2.5V,但是,我又在2.5V处,串接来个电阻对地,俩个电阻之间输出2V,但是在输出2V时,稳压端下降至2.45V,俩个电阻都是k欧姆级别电阻

    你的两个分压电阻的总阻值是多少?如果你要得到2V的精确电压,从2.5V往下分得总电阻得远远大于REF1004上端串接的50kohm电阻,这样的话,分压电阻的电流就不会对分压电路造成很大影响。

  • 由于REF1004内部是个稳压二极管,这样分压必须选择足够大的电阻,才不会对输出有影响。 带来的问题是阻值匹配问题,否则2V的误差比较大。

    建议可以选择REF3025或REF5025高精度参考,内部输出已经加有一级运放,外面电阻分压阻值就不需要太大。