This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

用TL494做同步整流问题

Other Parts Discussed in Thread: UCC24610

老师们好,我想用494做同步整流,我的设想是这样的: 首先让494输出一路PMW波,然后经过死区电路把494的输出波形分成两路,并带有死区。

最后将两路PWM波经过LM5100驱动后送往两个MOS管。

焊好板子后,我开始没让494工作,直接用信号源输出一路4V,50%占空比的方波信号给死区电路,然后通过调整信号源输出波形的占空比,

输出电压可调。

但是我加上494后电路就不能正常工作了。

现在我的问题有以下几点:

1、  494的输出波形的幅值是和输入电压相关的,可是我的死区电路用到7414,最大能承受的电压只有6V,我应该怎样把494的输出波形幅值限定在死区

电路正常工作范围内;

2、一般做同步整流的话,死区时间给多少比较好一点;

附上我的电路图,希望大家都帮我看一下。

Free Documents.pdf