Other Parts Discussed in Thread: UCC28070
问题1:UCC28070是固定频率工作再加拌动频率的工作方式吗?比如设置RRT电阻设置成130K,那么它的工作频率=7500/130=57.7K±10K工作方式吗?
问题2:UCC28070的CT是如何设计,它的磁芯饱和公式如何计算的?是以这个B_max=(L×I)/(Ae×N)吗,假如是,假如CT是200:1,那么此公式中的N=200,L是200匝的电感量,I是200匝副边的电流对吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
频率计算见datasheet 第15页。
变压器和耦合电感的磁性设计,TI没有提供相关文档(包括其他芯片也是没有提供的)。