我用TPS54386芯片做了一个15V转1.2V和3.3V的电源板,电感采用47uH,在实际测试时输出电压只有0.6V和0.45V,我去掉11脚电容后,1.2V电压正常,但是3.3V电压端为0.76V,之后用过各种手段,包括第15脚接地,去掉3.3V端稳压二极管,去掉3.3V端电感等,最后是3.3V端基本都去掉了(没有反馈了),电压在2.5V左右,按说应该是15V的百分之九十啊,也就是13.5V啊,怎么会是这个样子呢?可能是芯片坏掉吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用TPS54386芯片做了一个15V转1.2V和3.3V的电源板,电感采用47uH,在实际测试时输出电压只有0.6V和0.45V,我去掉11脚电容后,1.2V电压正常,但是3.3V电压端为0.76V,之后用过各种手段,包括第15脚接地,去掉3.3V端稳压二极管,去掉3.3V端电感等,最后是3.3V端基本都去掉了(没有反馈了),电压在2.5V左右,按说应该是15V的百分之九十啊,也就是13.5V啊,怎么会是这个样子呢?可能是芯片坏掉吗?
Qinyu
你好!
1. 关于15Vin转1.2V和3.3V的应用,你的电感选择过大,8uH左右感值,5A以上饱和电流的电感即可;
2. BP电容要按照手册建议典型值尽量靠近IC,不能去掉;
3. 你说的那个貌似不是稳压管,而是肖特基二极管。
下面有EVM的使用手册,跟你应用差不多,可以按照上面的指导画原理图和layout