看到BQ2022A EVM上面说可以支持1片或者两片编程,单独使用其中任何一个位置,软件都可以识别到,如果两片都同时插上,则软件无法识别到任何一片,如附件。想请教是什么原因? 谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Machael,
你好!请问如何对ID ROM进行编程, 我在BQ2022A EVALUATION SOFTWARE 上面没有找到。 谢谢!
Hi Michael,
我单独使用两颗BQ2022A在EVM上不同位置的时候,是能够读到不同ID的,所以我觉得ID ROM是不需要program的。
如果两片同时连接是无法搜索到ID的,两片同时在的话只能输入ID然后MATCH才能编程,谢谢。
不建议多片同时连接到总线上进行编程,推荐还是单片连接进行编程,效率会高点。
ID号获得:选择单片模式,EVM上只连接一片2022A,search 出ID号码记录下来。
连接2片2022A到EVM上,选择多片模式,输入ID号,点Select device按键就可以正常对该片进行编程了。
我这边用EVM尝试的是可以的。2片分开接在EVM上都能正常工作吗?确认下是否有管脚接反的可能?
其次,实际系统应用也是2片同时挂在单一总线上的吗?如果不是的话不建议在此花费过多的时间。