This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.TPS2376-H输出26W,CLASS等级电组应该为多少?
2.TPS2376-H和TPS2375芯片1脚ILIM外围连接电阻为什么不同?内部结构不同?TPS2376具有自恢复功能?
3.TPS2376-H芯片7脚UVLO可以悬空吗?
4.TPS2375预留的CLASS电阻255欧,电阻小于300欧时,没有电源输出?
着急购买芯片,谢谢专家回复!!!
山东烟台 王守朋 15153587623 邮箱wspytu@163.com
王工,请参考以下回答:
1.TPS2376-H输出26W,CLASS等级电组应该为多少?
接255ohm (class4), 或者由PSE侧重新定义。
2.TPS2376-H和TPS2375芯片1脚ILIM外围连接电阻为什么不同?内部结构不同?TPS2376具有自恢复功能?
ILIMI外围连接电阻不同是由于内部的电流采样电阻不同,TPS2376-H是50mohm,TPS2375是80mohm。 TPS2376过热关断后有自动重启功能。
3.TPS2376-H芯片7脚UVLO可以悬空吗?
不可以。要接Vin下来的分压电阻。
4.TPS2375预留的CLASS电阻255欧,电阻小于300欧时,没有电源输出?
255ohm是class 4. 此场合取决于PSE, 如PSE 为TYPE1, 不支持高功率,则没有输出, 若为TYPE 2型,支持LLDP并与PD端通讯上, 则可以上电。若为2 event 检测,则不上电。