This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于UCC28019的问题跪求解决

我的设计目标是,输入电压11v ac,输出电压24Vdc,Pout=24W,有几个问题想请教一下各位:

1.输入端的共模扼流圈一定要加吗?

2.mosfet门极电阻上并联的这个稳压管是什么作用?

3.电感前,整流桥后的波形怎么会像被叠加了一个5v的直流电压,在5v的     基准上出来的正弦半波?

4.判断电路是否正常工作,除了输出电压不随负载变化,稳定在24V之外,是不是采样电阻R5的左端的波形应该是负的连续的正弦半波,相位和整流后输入端相位相同?

望能一一解答,盼复!

 

 

  • 4..判断电路是否正常工作,除了输出电压不随负载变化,稳定在24V之外,是不是采样电阻R5的左端的波形应该是负的连续的正弦半波,相位和整流后输入端相位相同?

    应该是三角波,和开关管的栅极驱动电压同相位。

  • 3.电感前,整流桥后的波形怎么会像被叠加了一个5v的直流电压,在5v的     基准上出来的正弦半波?

    可以检查一下输入AC的幅度吗?按照你所说的,如果是11VAC整流之后不应该是只有5V+纹波。

    你看了这个正弦波的频率没有?如果是输入AC频率的两倍,那么就是正常的整流波形,如果频率不是2倍的关系,说明环路没有稳定,需要仔细检查布板,调整反馈环路;

  • 为什么会是三角波呢?PFC的目的不是校正主电路的电流让它跟随正弦半波吗?