This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI电源芯片在PSR方面的应用



TI电源芯片可有小瓦数的PSR方面的应用,或者PSR+PFC方面的应用,如果有,与其他的相比的优势在哪呢?

  • 你好:

            UCC3809可实现小瓦数的PSC应用。

    1、它们是经济型低功耗集成电路包含所有控制与驱动电路;内部实施的电路包括:启动电流不到100μA的欠压锁定、用户可接触电压基准、确保闭锁操作的逻辑元件、PWM比较器,以及吸入或输出峰值电流的图腾柱输出级(totem pole output stage)。

    2、振荡器频率与最大占空比可通过两个电阻器与一个电容器进行编程。UCC3809系列还具有全周期软启动。该产品系列具有适用于离线式与DC/DC系统的UVLO阈值与滞后级别。

    3、UCC3809具有SOIC(D)、PDIP(N)、TSSOP(PW)与MSOP(P)封装。其小型TSSOP与MSOP封装使得该器件理想适用于板级空间与高度极为有限的应用。

    www.ti.com/.../ucc3809

    www.ti.com/.../sluu087b.pdf