This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5118低电压输入时带负载能力差

Other Parts Discussed in Thread: LM5118

我用LM5118做了一个6-50输入12v3A 输出当电压在15v以上输出电压正常,当电压在低于15v输出的电流很小不到1A,负载大的时候就把输入电压都拉低了

  • 你好

    是不是输入电压带电流能力不够,如果15V输入,12V,3A输出,这时的输入电流大于2.5A,请确认实验用DC SOURCE有3A的驱动能力。

  • 输入电压都被拉低了,请考虑输入电源的带载能力。

  • 请检查输入电源的功率,另外,输出负载是否可调, 请确认输出在什么点到时候出现异常?

  • Hi

           按照您15V以上的输入都没有问题,也就是说您的电源供应器带载能力超过12*3/15/0.85=2.8A(或者说42W,且实际效率应高于85%),  所以电源供应器应该是没有问题的。

           按照电流限制2.8A, 当输入为10V时, 10*2.8*0.85/12=2A, 应该不止1A.

           请将你的电路传上来看一下。也可以确认一下你的电源供应器是否限流到3A,同时确认一下输入电容(输入电容足够大,靠近MOS,layout走线较宽)

           需要说明的是,在输入15V时,这个时候差不多将进入buck-boost模式了,电感的峰值电流将会上升很多,也就是说本来buck电路输出3A时的峰值电流,在buck-boost电路中1A左右甚至不到就可以达到了。所以你需要确认你的电感饱和电流足够大,因为只有电感饱和了,才会有机会超出较大的功率而降电源供应器的电压拉低。

  • Hi

       如上所说,这其中也会造成另一个问题,就是进入buck-boost模式后,会有较大的输入电流,不少电源供应器的最大电流时在3A, 你需要确认。