This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5450用TPS5430替换问题

Other Parts Discussed in Thread: TPS5430, TPS5450

之前做过TPS5450,现在需用TPS5430来做。看datasheet发现TPS5450和TPS5430的引脚也兼容,就是推荐的Layout不一样。请问将TPS5430用在TPS5450的Layout上会不会有问题(设计参数都满足TPS5430的工作条件),感觉应该不会,还是上来问一下。

  • Hi

       TPS54X0(X=1,2,3,5)为一个系列的不同产品,主要差别在于内部MOS的电流规格不同,TPS5430是3A最大输出,而TPS5450是5A输出。

       因此在TPS5450的layout基础上用TPS5430是完全没有问题的。(因为两者的热阻是差不多的,但是TPS5450带的负载比TPS5430大,因此功耗也大很多,如果它的layout能满足这个功耗产生的热,对于使用TPS5430是绝对没有问题的)

       需要指出的是datasheet中之所以出现layout的差异是因为TPS5430采用的是双层板,所以与芯片PowerPad焊接的可视GND面积非常大(用于散热),而TPS5450采用的是4层板,在正面看起来与芯片PowerPad焊接的可视GND面积比较小,但是其他几层连接GND的散热面积是非常大的。

  • Hi

         不客气。

         其实你还可以直接焊接上去测试看看,主要是确认芯片温度。

  • 嗯,板子是按照TPS5450做的,对TPS5450效果挺好的,温升也不高。今天下午用TPS5430试过了,没问题。