我参照TMDSSK3358开发板基础上设计一个产品,但需要增加电池及充电功能,初步想用一个3000-4000mah的锂电池。
BeagleBoneBlack上所用的PMIC支持充电,但从TPS65910A3更改到TPS65217C,工作量有些大。因此我想直接在TPS65910A3基础上增加一个充电芯片,不知那款充电电池芯片较为合适?谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我参照TMDSSK3358开发板基础上设计一个产品,但需要增加电池及充电功能,初步想用一个3000-4000mah的锂电池。
BeagleBoneBlack上所用的PMIC支持充电,但从TPS65910A3更改到TPS65217C,工作量有些大。因此我想直接在TPS65910A3基础上增加一个充电芯片,不知那款充电电池芯片较为合适?谢谢。
请问能否提供其他比较详细的信息,比如输入输出电压是多少,充电电流多少,需要主机控制还是standalone,以及是否需要DPM?
Sheldon,谢谢您的回复。
输入电压时适配器供电5V,电池充电电压为4.2V,充电电流最好能达到2A左右。主机控制和standalone控制均可,最好有DPM。
我看了BQ2416x应该能符合要求,但它是双输入的。我这个应用不需要USB充电,请问是否有更适合的推荐,谢谢。
另外请问我在使用电池供电时(一般锂电池输出为3.7V),若还想使用USB接口,则是否还需要设计一个boost电路将3.7V转为5V?