When we use BQ76952 to get 16 channel cells voltage and 5 channel temperature, we must get these data in 100 ms. There is a question that when we get voltage and temperature according to full scan flag of alarm status, we should take 194 ms to confirm the full scan flag become 1 from 0. We hope to get voltage and temperatue according to adscan flag of alarm staus , we find that there is only 65 ms for ad scan flag to becom 1 from 0. Pls help us to confirm that we can use ad scan flag or not.