This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

试图在4-20mA电流环路上串联一个稳压电源并用SN6501产生一组隔离电源但不成功。

Other Parts Discussed in Thread: SN6501

试图在4-20mA电流环路上串联一个稳压电源用SN6501隔离后提供3.3V给ADC工作。ADC消耗的电流约为3.3V/1.5mA.试过多种稳压方案无论负载电流大小均被SN6501钳位于1.6V左右。SN6501单元电路在其他电源上工作正常。我的问题可能是所制作的稳压电源满足不了SN6501对输入电源负载能力的要求。请问该如何设计该稳压电源?

  • 这种环路电源要考虑实际供电能力,一般最大20v,可吸取电流3ma,大致可以按照5v3ma来制作,因为环路设备有可能不止一个,并且环路电源可能为12v,那么按照两个设备,那就是10v,达到最大能力了,所以你的电源只能吸取15mw,也就是说足够你的adc用,主要是你的电源的设计问题,这种环路窃电还是比较成熟的。

  • Hi

        在你的这个电路中,输出只能达到1.6V, 而SN6501的输入电压输出电压是通过变压器咋比固定的,也就是说你的输出达不到预定的3.3V很可能是因为SN6501输入达不到预定的输入值,也就是说不可以简单的采用串联SN6501的方法, 而也需要将输入电压箝位到预定的输入值范围内(或可以采用低功率的LED二极管之类,因为它的导通压降刚好可以是3.3V,也就是说可能将SN6501串联输入箝位到3.3V)

        没有实际这样做个,以上仅仅为个人意见,有不对的地方可以讨论。