求推荐一个能输出-10V,输出电流达1A左右的转换器
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
输入电压是多少? 用降压芯片都可以做,可以参考设计文档: www.ti.com.cn/.../slva257a.pdf
HI
如上文档,你需要选择输入大于22V以上的电源芯片,如上TPS5430刚好合适。
如上面文档,最大输出电流为原芯片最大输出电流Io的1-D 倍, 也就是说你需要2A最大输出,那么如果你10V输入,你需要选择最大电流为4A以上的降压芯片来做。