This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于LDO的问题



最近使用了一款TI的LDO,遇到点问题:

按照规格书要求是:输出3.3V,最大电流可到800mA,但是输入要求4.7V以上。

请教一下,如果我的输出电流只有200mA,但是输入只有4.5V,那么这个LDO是否可以正常工作?