Other Parts Discussed in Thread: BQ25060, BQ24060
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
若你系统供电电压范围比较宽,是可以这样使用的。但更推荐带电源路径管理的,可以将系统供电电压维持在较小波动范围内,如BQ25060。
Thanks!
谢谢!
为什么要有较宽的供电电压?
我这个系统是5V的适配器供电,然后机器一边充电,一边工作,这种情况下是由电池供电还是由5V适配器通过BQ24060供电?
BQ24060不带Power Path功能,不支持一边充电一边给系统供电。
建议采用带有DPPM功能的充电芯片。
因为在电池充电过程中,受电池电压限制,BQ24060的输出电压会是电池电压值,而电池充电过程中电压变化范围比较大,所以就需要你的系统工作电压范围比较大(至少在电池充电电压范围内都能正常工作)如果能正常工作,那么就可以一边充电一边给系统供电,在这个过程中,系统工作需要的能量由BA24060提供,多余的能量给电池充电。