This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3842启动疑惑

Other Parts Discussed in Thread: UC3842

网上看了一篇文章说:“当HV+电压建立后,首先通过启动电阻R1R2提供电流给电容C1充电,C1电压逐渐升高,当C1电压达到UC3842的启动电压门槛值16V时,UC3842开始工作并提供驱动脉冲,由6端输出推动开关管工作,在这个过程中,由于R1R2提供的电流不足以维持UC3842的工作电流,因此电容C1放电,电容电压逐渐降低,在电容电压降低到3842的截止工作电压(10V)之前,辅助绕组必须提供IC工作的电压。也就是说在电容C1电压降低到10V之前,辅助绕组通过D1R3整流后的电压必须超过10V,否则UC3842C1上电压降低到10V后会停止工作,然后输入电压又通过R1R2  充电,电容电压升高到16V,周而复始,重复启动。”

我记得身边的人说过刚开始经过启动电压供电后,后面就是靠辅助绕组供电了,为什么会重复启动呢

  • 在UC3842的C1电压跌到截止电压以前;变压器产生的辅助电源电压能达到截止电压,辅助电源就会接过接力棒;由辅助电源供电(呵呵!毕竟C1供电和辅助电源是线或的;谁高就依谁)。如果辅助电源达不到截止电压而电容电又放到下限,UC3842就会打嗝。

    因此;你的听说是对的;是正常过程。但是;如果你拿这样的电源带满载启动,就会启动失败而“打嗝”。

  • 重复启动的前提是:电容C1上的电压降低到IC启动电压之前,辅助绕组提供的电压没有达到IC工作电压。简单的说,就是辅助绕组没有提供能量,那么只能重复启动了。