This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895: 充电问题:关于寄存器配置好充电截止电流后,充电电流不能达到设定的值

Part Number: BQ25895

你好!

    问题:寄存器配置为充电电流限制为2.4A,但实际充电电流只能到1.6A左右,电流无法提升。

              但是改变寄存器的电流限制为1.2A,实际测试是可以达到1.2A左右,就是设置的电流限制超过1.6A后,就无法达到设置的充电电流。  想请问一下是什么原因造成电流上不去的呢?

               在充电时,寄存器状态是如下:

           

    寄存器配置如下:

           REG00:70

           REG01:06

           REG02:3D

           REG03:3A

           REG04:26

           REG05:18

           REG06:5F

           REG07:B9

           REG08:00

           REG0A:C3