This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25890: 过放电池充电异常

Part Number: BQ25890


你好!

帮忙分析解决下,谢谢!

1、使用QC2.0充电头时,BQ25890在给过放电池充电情况下,REG0B寄存器的vbus_stat值不是b100,充电头输出只有5v,不会切换到12V输出

2、REG02寄存器的FORCE_DPDM位置1后,充电头输出始终是5V输出,FORCE_DPDM位不会返回0,充电电流会降为0,会停止充电

  • 您好

    1, 应该是没有握手成功所以不能输出高电压,请确认MAXC_EN or HVDCP_EN是否使能。

    2,不需要强制执行 D+/D- 检测,如果 D+/D- 线连接正确且 HVDCP_EN 位已设置,则主机无需干预插入时的 USB 检测