This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR14020-Q1: RT/SYNC设置开关频率的问题

Part Number: LMR14020-Q1


根据LMR14020-Q1的手册图17. synchronizing to an external clock

"When using a low impedance signal source, the frequency setting resistor RT is connected in parallel with an AC coupling capacitor CCOUP to a termination resistor RTERM (e.g., 50 Ω). The two resistors in series provide the default frequency setting resistance when the signal source is turned off."

1. 低阻抗时钟源为什么要按照左图连接?没有理解其中含义。

2. 如果FPGA输出时钟作为clock source, 是高阻抗还是低阻抗呢?

3. 我希望实现:有外部时钟源的时候开关频率和外部时钟源一致,没有时钟源时按照RT设置默认的频率。左图和右图均可实现吗?手册原文中,好像只有左图可以实现。

  • HI

        1. datasheet没有提及高低阻抗时钟源的特性,但是外部时钟电路本质都是要尽量减小异常的震荡,和提供稳定的CLK源。

        2.PFGA的CLK源,建议直接看看其datasheet推荐。

        3. 一般是二选一设置频率,你可以看看datasheet里面是否提及,是否有主副频率设置,例如当SYNC芯片高于RC频率设置时,可实现SYNC频率同步。如果有提及,就可以实现,但前提如上所提,你所提供的SYNC频率会比RC频率高。