Other Parts Discussed in Thread: UCC28710, UCC28019, UCC25600, UCC28250, UCC28051, LM5025
要求:
1.参数:交流输入范围220V+20%,输出24V、5A,最大纹波电压100mV,工作频率100kHz
2.电路:桥式整流,大电容滤波,DC/DC采用半桥,主功率管为MOSFET
我初学者,请问这样的电路应该选用哪款芯片呢,有没有成型的方案可以借鉴呢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果是一级电路可以考虑一下ucc28710的方案- http://www.ti.com/tool/pmp9041
如果是两级电路可以参考一下这个设计- http://www.ti.com/tool/pmp5141
Hi
如果您采用半桥目的是高效率,或可以采用LCC半桥谐振芯片UCC25600, 前面用UCC28019做PFC: http://www.ti.com.cn/product/cn/ucc25600
你好,
推荐前面加PFC,用UCC28051。后面的半桥芯片推荐LM5025(A/B/C)或者UCC28250,你也可以考虑LLC UCC25600。
这种复杂电源的设计用Webench设计不合适,每个产品的主页面都能下载到专门的设计软件,一般是Excel做的。