Other Parts Discussed in Thread: TPS23754
tps23754启动电流偏高,0.1A 以上,IC 发烫,输出电压很低,采用EVM-383参考电路,VC启动电压升高到10V后呈三角波,这是什么原因?CLS到地的电阻我选择了56欧姆,会影响到启动电流吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1:如果只是调试PSE部分,不带PD功率级,class电阻可以不用连接吧?
class电阻可以不连接。你把PSE设置成semi-mode就可以看到端口一直出现检测和分级的信号。
2:我把TPS23754的APD直接接RTN,而PPD直接接VSS,把PD的部分断开,其他参数完全按照383 DEMO参数设置,仍然不能启动,难道必须连接PD级吗?难道必须要有回授信号才能启动?如果必须要回授信号,那就是PD的输出电压不高引起的,我现在输出电压只有2V,而且因VCC 电压不稳定而变化。
建议首先检查PD的各个引脚对地的阻抗,然后用DC source48V 作为输入,断开L1电感,上电,检查PD各个引脚的波形,重点查一下VC 和VB引脚。
TPS23754没有semi-mode,在PSE端才有的。
请问你采用的那颗PSE?
TI的PSE请参考:http://www.ti.com/lsds/ti/power-management/power-sourcing-equipment-products.page?paramCriteria=no
你好,我的问题跟你的一样,方案是一样的,不断的启动,VC电压是锯齿状的,当时你是怎么解决的呢