Part Number: UC2845
UC2845的震荡频率参数如规格书上下图所示,PWM波形频率为震荡频率一半。现实际使用参数Rt=10k,Ct=1nF,测试PWM输出频率在86k左右,为正常;测试发现当Rt=20k,Ct=0.47pF时,输出频率在184k左右,为理论值的一倍,这是什么原因?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: UC2845
UC2845的震荡频率参数如规格书上下图所示,PWM波形频率为震荡频率一半。现实际使用参数Rt=10k,Ct=1nF,测试PWM输出频率在86k左右,为正常;测试发现当Rt=20k,Ct=0.47pF时,输出频率在184k左右,为理论值的一倍,这是什么原因?

HI
PWM频率86kHz, OSC频率186kHz, PWM波形频率为震荡频率一半, 能否将波形传上来看看?
HI
从测试看,与2倍整的关系略有差异是很可能是示波器测试OSC频率会有寄生参数的影响会略有偏差,而PWM则没有这一问题。
你好,不是这个意思,就是Rt1=10K,Ct1=1nf和Rt2=20K,Ct2=0.47nf的条件下,理论上输出的PWM波形频率应该是一致的,为什么会出现测试条件2的时候,输出频率是第一个的2倍左右?
HI
是的,我写错了,如最上面你所说测试PWM输出频率在86k左右,为正常。
按照公式2中情况下频率是应该一样。在同一个板子上两种配置频率差异显示异常,如上我提到如果改回改变回Rt1=10K,Ct1=1nf,频率会正常吗? 我担心在更换过程中是否有可能导致芯片损坏?