请问谁有bq76pl536故障恢复程序,我的芯片进入故障状态了,现在急需恢复正常,该怎么办?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
帮你把这个case转到电池管理里面(原因是几天前就看到这个帖子,但是没有工程师回,可能是因为熟悉电池管理的工程师没有到电源管理脸面看到这个case)
你好,在你的另外一个帖子已经回复了。如果你会读写相关寄存器应该编写这个程序不会有太多难度。
datasheet里有这样一段话,就是需要对相应的错误寄存器FAULT_STATUS 或 ALERT_STATUS 写1来清除。Fault Recovery Procedure When any error flag in DEVICE_STATUS[], FAULT_STATUS[], or ALERT_STATUS[] is set and latched, the state can only be cleared by host communication via SPI. Writing to the respective FAULT_STATUS or ALERT_STATUS register bit with a 1 clears the latch for that bit. The exceptions are the two FORCE bits, which are cleared by writing a 0 to the bit. The FAULT_STATUS[] and ALERT_STATUS[] register bits are read-only, with the exception of the FORCE bit, which may be directly written to either a 1 or 0.