Part Number: TPS40170
请问TPS40170在无负载的情况下(不抽电流),工作结温70℃正常吗?
抽载7A电流时,TPS40170的工作结温也是70℃。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
芯片官网有在线仿真webench,可以借助这个工具确认芯片结温。
对于芯片温度偏高,首先建议选择Qg尽量小的MOS, 其次工作频率不要太高(推荐300kHz左右)。芯片底部PowerPower充分与GND焊接,并且扩展GND面积用于散热。
HI
一般推荐不并联MOS来增加负载能力, 有这样做的,但是很少,要不然也不会采用laod share并联芯片来做。
虽然datasheet没有提及,但TPS40170这颗芯片的驱动能力应该并不强。