This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps54620输出电压的调整电阻?

Other Parts Discussed in Thread: TPS54620

12V输入, 输出1.1V, 3A

TPS54620建议的R6的值是10K,

我现在必须要用R6=18K, R5=6.8K, 这样是否可以? 是否会不稳定?