This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用TPS63060做恒流驱动,输入3.2V, 输出驱动单个LED, LED偏置电压2.8~3.0V, 想把驱动电路设定在600mA左右。
按照应用手册Different Methods to Drive LEDs Using TPS630xx Buck-Boost Converters, http://www.ti.com.cn/cn/lit/an/slva419b/slva419b.pdf
电路A: 输出498mA很稳定,效率68%;
电路B:输出电流初始值230mA,10分钟后,输出电流稳定在633mA,效率85%;
电路C:输出电流初始值521mA,10分钟后,输出电流稳定在670mA ,效率82.2%(不能理解为什么还是需要一段时间让输出电流稳定).
电路C是A(稳定)和B(效率)的折中选择,我现在的问题是如何能用电路C让输出电流在几秒钟就达到稳定值?
或者有没有其他的电路可以实现2.5V~9V输入,驱动单个LED,驱动电流600mA左右。
谢谢!