Other Parts Discussed in Thread: BQ35100
- Part Number: BQ35100
1、如果我设置检流电阻为100mΩ时,最小能检测到的最小电流是多大?能检测到8uA/2ms的电流么?
2、如果我设置检流电阻为25mΩ时,最小能检测到的最小电流是多大?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,已经在E2E英文论坛发帖,请继续关注。
For the correlation between the sense resistor and minimum sensible current for this device, it is the voltage generated by an 1mA flow through a 4.768mOhm sense resistor, when using a 100mOhm resistor, a 4.768uV LSB is 0.048mA current, but it would be only displayed as 0 in Current() register until the actual current is greater than 1mA